Install InfoPlatform

FactoryTalk Analytics InfoPlatform service supports FactoryTalk Service (For Example: Historian, OPCUA, InfluxDB, PIAF, etc) and FactoryTalk Edge Gateway Connectors (For Example: InfluxDB2). This is optional and a separate executable must be downloaded from Rockwell Software download site:
Refer to “
4.00.00_FactoryTalk Analytics InfoPlatform Service Installation and Configuration Guide
”.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.