Verification Step
- Verify the installation directory with the figure below:Directory
- Open the Windows Services console. Ensure the following services are installed:
- FTAnalyticsDataView
- FTAnalyticsDataImporter
- Elasticsearch
- FTA Security
- PostgreSQL
- FactoryTalk Activation Helper
- FactoryTalk Activation Service
- FactoryTalk Activation Websocket ServiceWindows Services Console
Provide Feedback