Elasticsearch Index Naming Convention

Elasticsearch Index Naming Convention

The following types of indexes are created by DataView in Elasticsearch:
  • Temporary Index
  • Re-Index
  • CSV Connector Index
  • Save Story Board Index
  • Force Index
The following table details the Elasticsearch index naming convention for Normal Index and Purge Index:
Index Type:
Temporary Index
Syntax
"cielasticsearch_" + clientID + "_" + "temp_" + userID + "_" + clientID +"-" clientID+userID + DateTimeFormat.forPattern("YYYY.MM.dd-HH.mm.ss.SSS").print(now) + "-1";
Example
cielasticsearch_1_temp_5001_1_15001-2022.09.13-08.24.56.542-1
Index Type:
Re-Index
Syntax
"cielasticsearch_" + clientID + "_" + "temp_" + userID + "_" + clientID +"-" + DateTimeFormat.forPattern("YYYY.MM.dd-HH.mm.ss.SSS").print(now) + "-1";
Example
cielasticsearch_1_temp_3_1-2021.10.21-05.58.11.719-1
Index Type:
Save Dataset Index
Syntax
"cielasticsearch_"+ clientID +"_report"+ clientID +"_"+ generateDatasetId+ DateTimeFormat.forPattern("YYYY.MM.dd-HH.mm.ss.SSS").print(now) + "-1"
Example
cielasticsearch_1_report_1_6176-2022.04.28-07.10-1
Please Note:
  • In the above syntax, "now" indicates Current Date and Time.
  • In the above syntax, "Mills" indicates Current Time in milliseconds.
  • To identify the Normal Index name related to the Dataset, user can refer index_name column of in_direct_elastic_search table.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal