Change Dataset

Change Dataset

Perform the following steps to change the Dataset of the Storyboard:
  1. Click [Change].
    Change Dataset
    The Choose Dataset page displays.
  2. Select the desired Dataset from the drop-down list.
  3. Select the checkbox, if User wants to set the selected Dataset as default Dataset.
  4. Click [Select], the Chart settings window displays.
    Select Dataset
    IMPORTANT:
    All the attributes like X-Axis, Y-Axis, Tooltip, Reference line, Sorting & Ranking reset to empty values, User can change the attribute configuration as required. The Chart Type and Style remain the same.
  5. Navigate to the Configuration tab, click the [] icon and select the X-Axis and Y-Axis attributes from the drop-down list.
  6. Click [Apply].
    NOTE:
    If the X-Axis and Y-Axis attributes are not selected then the ‘Configure the Axes for this chart to update.’ message displays.
    Configuration Settings
    The Chart with updated Dataset displays.
  7. Click the [] icon to minimize the chart tile.
  8. Click [Save Changes] to save the Storyboard.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.