X-Axis
- Under the X-Axis, Select the desired attribute using the [
] icon.
- User can toggle the Display X-Axis Label using the slider. By default, it is turned on.X-Axis
For any chart, if multiple data is selected on X-Axis a warning message with particular chart name displays.
Multiple X-Axis Warning Message

- Perform the following steps to change the X-Axis column:
- Click the [
] icon and select [Remove] to delete the column.
Delete X-Axis - Click the [
] icon to select column from the drop-down list.
Add X-Axis - Click Apply, updated chart displays.Updated Chart
Provide Feedback