Ranking

Ranking

  1. Select whether ranking should be done from Top or from Bottom.
  2. Define the number of records to be displayed. User cannot enter 0 in the number of records displayed section.
    IMPORTANT:
    Ranking is only applicable for fields in Y-Axis.
    Ranking
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal