Absolute
The function of “Absolute” is to return the absolute value of a numeric input argument.
Syntax
: absolute(field_name) Example
: absolute([rental_rate]) It will give the absolute value for the given field.
Provide Feedback