Math.atan
The function of “atan” is to return the arc tangent of a number (number field). It returns the arc tangent of an angle, in the range of -?/2 through ?/2.
Syntax
: math.atan(field_name) Example
: math.atan([rental_duration])Special cases
: - If the argument is NaN, then the result is NaN.
- If the argument is zero, then the result is a zero with the same sign as the argument. A result must be within 1 ulp of the correctly rounded result. Results must be semi-monotonic.
Provide Feedback