Math.Cos
The function of “Cos” is to return the cosine of a given field. A numeric value used to calculate the Cos. It is an angle expressed in radians.
Syntax
: math.cos(field_name) Example
: math.cos([rental_duration])Provide Feedback