Math.Floor
The function of “Floor” is to round the specified number down and return the largest number that is less than or equal to the specified number.
Syntax
: math.floor(field_name) Example
: math.floor([rental_rate])Provide Feedback