StartsWith
The function of “StartWith” is to test if this field starts with the specified suffix. It returns "true" if it starts with the suffix otherwise it returns “false”.
Syntax
: startswith(field_name, “String”) Example
: startswith([special_features]“A”)Provide Feedback