Substring

Substring

The function of “SubString” is to get a substring of a field by indicating the start and end position from the beginning of the field.
Syntax
: substring(field_name, int start, int end)
Example
: substring(field_name, 0, 4)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal