Bar Time Series Chart

Bar Time Series Chart

Time Series Bar Charts are used to show the changes in a metric over time as a series of bars. User can also graph multiple series this way, to show the breakdown of a metric across dimensions, and how the values change over time.
  1. Open a Storyboard, hover the mouse on a chart tile and click the [] icon to maximize the tile.
  2. Click the [] icon. The Chart Settings window displays.
    View
    Under the Type tab, the list of available chart types display.
  3. Click [Bar Chart]. The available chart models display.
  4. Select the [Bar Time Series] chart from the Bar Chart section.
    Chart Settings
    IMPORTANT:
    A Warning message displays when Time Series chart is selected.
  5. Under the Configuration tab, provide the following properties:
    • Y-Axis: Select the desired attribute using the [] icon. User can select multiple Y-Axis values for this chart.
    • X-Axis: Select a date attribute on X-Axis to generate Time Series chart, by using the [] icon.
      NOTE:
      An error message displays if the date attribute is not selected on X-Axis.
    • Legend: Select the desired field from the drop-down list to apply a different series on top of X-Axis or Y-Axis for comparing the available data.
    • Tooltip: User can select the values to be displayed on the tooltip.
    • Min/Max: User can select the Minimum and Maximum values to display on chart.
    • Reference Line: User can set the properties to view the Reference Line on the Chart.
      NOTE:
      The Reference Line option is not available, if the Storyboard is generated with direct query.
  6. Under the Style tab, User can change the following:
    • Chart Theme: Change the theme color.
    • Chart Settings: User can enable or disable the following options:
      • Chart Title, Cross Hairs, Data Label, and Grid Line.
  7. Click [Apply].
    Chart Settings
    The Time Series Bar chart displays.
    Time Series Bar Chart
  8. Click the [] icon to minimize the chart. The updated Storyboard displays.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal