Combination Chart

Combination Chart

Enables user to combine several chart types in one chart.
  1. Open a Storyboard, hover the mouse on a chart tile and click the [] icon to maximize the tile.
  2. Click the [] icon. The Chart Settings window displays.
    Chart Settings
    Under the Type tab, the list of available chart types display.
  3. Select [Combination Chart].
    Select Chart Type
    If user tries to click Apply “The Combination chart requires at least two Y-Axis” message displays.
    Multiple Y-Axis Error
  4. Under the Configuration tab, provide the following properties:
    • Y-Axis: Select the desired columns and set the aggregation using the [] icon. User can add more than one Y-Axis values for this chart.
    • X-Axis: Select the desired attribute using the [] icon.
    • Tooltip: User can select the values to be displayed on tooltip.
    • Reference Line: User can set the properties to view the Reference Line on the Chart.
      Chart Settings - Configuration
  5. Configure the Combination Chart list settings, the selected Y-Axis columns displays:
    • User can select the position of the column and can change the chart type.
    Chart Settings
  6. Under the Style tab, User can change the following:
    • Chart Theme: Change the theme color.
    • Chart Settings: User can enable or disable the following options:
      • Chart Title, Cross Hairs, Data Label, and Grid Line.
  7. Click [Apply].
    Chart Settings
    The Combination chart displays.
    Chart Settings
  8. Click [] icon to minimize the chart. The updated Storyboard displays.
    Storyboard Updated
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal