Delete Dataset

Delete Dataset

Perform the following steps to delete a Dataset:
  1. Navigate to the Connections tab.
  2. Expand the folder where the Connection is added.
  3. Click the [] icon corresponding to the dataset to be deleted and click [Delete].
    Delete Dataset
    The Dataset deleted successfully message displays.
  4. The Delete Dataset dialog displays. Click [Delete] to delete the dataset.
    NOTE:
    This action will delete the dataset and user cannot restore the dataset.
Delete Dataset
The
"Dataset deleted successfully"
message displays.
NOTE:
If a dataset is used in multiple Content and user try to delete the same dataset then an error message displays.
Error Message: Multiple Content Datasets
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal