Supported Connectors
DataView supports the following connectors listed below. Refer to the
4.01.00 FactoryTalk Analytics DataView Connectors Configuration Guide
for further details.List of supported Connectors:
- Rockwell Automation
- FactoryTalk Service
- FactoryTalk Edge Gateway
- FactoryTalk Metrics
- FactoryTalk Alarms & Events
- Database
- SQLServer
- FlatFiles
- CSV
NOTE:
For compatibility, it is recommended to use the following versions of software to work with DataView 4.01.00:
- FT Metrics Version 13.00.00
- FT Alarms & Events Version 6.21.00
Supported Connectors

Refer to Appendix A, “Supported Features - Direct Query and Non-Direct Query” section for supported features.
Provide Feedback