Exclude Filter
- Click on a data point of any chart, the Data point Quick Access menu displays.
- Click the [
] icon to apply Exclude filter on the dataset.
Quick Access MenuThe filter [] icon displays on the updated chart(s) of a Storyboard.
NOTE:The applied Filters are listed under the Instant Filters section.Exclude filter - Click the [
] icon to [Save Filter] or [Delete] the filter.
- Select the [Exclude NULL Values] checkbox to exclude the null values from the Storyboard.
- Close the Filter window and click [Save Changes] to save the Storyboard with the applied filters.NOTE:The Quick Access Menu may vary based on the connector. For example, few features of Quick Access Menu for FT Service and FT Edge Gateway will be disabled.
Provide Feedback