Mapped Filters
Mapped filters option is available only for the Storyboards created with pre-configured templates. Allows User to apply filter with more than one column from multiple datasets.
Example: For Mapped filter if Shift column is selected it applies to the dataset1.shift, dataset2.shiftname columns in different datasets.
- On the Storyboard, click the [] icon.The Filter window displays.
- Click [Add Filters] and the Choose a Filter dialog displays.
- Under Column Mapping section select the required columns and click [Next].NOTE:Mapped filter does not have Numeric field in Column Mappings.NOTE:User can select multiple columns for Column Mapping. If the selected columns have a large data, it takes time to load the page.
- Click the [] icon and select the columns to apply filters.
- Click [Add].NOTE:The [Apply] option is enabled only when the new columns are added, or existing columns modified in order to apply filter. Once the filter is applied, the [Apply] option is disabled.
- Click [Apply].
- Click [Multiple Datasets] to view the column Mapping details.
- Click the [] icon to close the Filters window.The Storyboard with applied Filters display.
- When the User changes the dataset for any chart tile the Mapped filter on the chart is updated.
- Click [Save Changes] to save the Storyboard with the applied Mapped filters.
Provide Feedback