General Settings

General Settings

  1. Edit the following options from General Settings section:
    • Content Name:
      Enables the User to edit the Storyboard Name.
    • Favorite:
      Displays the Content that are marked as favorite. User can click the [] icon to mark Content as favorite or click the [] icon to remove from favorite.
    • Containing Folder:
      Select the folder from the drop-down list or create a new folder, to change the folder where the Storyboard is saved.
    • Navigate to Content:
      Select the Content from the drop-down list that the User will be able to navigate to. This will cause an association from the current Storyboard to the selected Content. Click the arrows on the bottom right corner to navigate to the linked Content.
    • Time Zone Settings:
      Select any of the following timezones as per the requirement:
      NOTE:
      If the User changes the Timezone, the Date Filters that are already applied to the Storyboard will be removed.
    • Local Time Zone:
      Enables User to select the local time zone where the Client / User node is located.
    • Source Time Zone:
      Enables User to select the time zone where the Data Source is located.
    • UTC Time Zone:
      Enables User to select the UTC time zone.
    • Other Time Zone:
      Enables User to select the desired time zone from the drop-down list.
    Storyboard Preferences - General
  2. Click [Reset Settings] to change it to original settings.
    (OR)
    Click [Apply] to apply the changes.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.