FTEGInfluxDB Model
The FTEGInfluxDB server model contains:
- Databases: Bucket is mapped into database. It is a logical container for users, retention policies, continuous queries, and time series data.
- Measurements: The Model of FTEDGE Gateway as a measurement is the part of FTEGInfluxDB structure that describes the data stored in the associated tags.
- Tags: The key-value pair in FTEGInfluxDB data structure that records metadata and the actual data value. Here is a typical FTEGInfluxDB model:FTEGInfluxDB - Tags
Provide Feedback