Custom Query Support
The InfluxDB connector supports the usage of the Influx Query Language (InfluxQL).InfluxQL is a SQL-like query language for interacting with data in InfluxDB. The connector offers the operation “ExecuteQuery” on the InfluxDB server item. The input parameter is a string that contains the query.
InfluxDB Server Properties
![](/content/dam/dita/en/factorytalk-analytics-dataview/4-01-00/infoplatform-guide-01/configure-infoplatform-service/influxdb3.png/_jcr_content/renditions/original)
Provide Feedback