Subscription
Support
InfluxDB subscriptions
are local or remote endpoints to which all data written to InfluxDB
is copied. InfoPlatform provides a web server endpoint as a callback
endpoint to be informed by InfluxDB on all field and tag value changes.
The configuration of the endpoint must be done for every InfluxDB
server separately. See configurations section for more details.
Provide Feedback