Verify InfluxDB Tags

Verify InfluxDB Tags

  1. Log in to DataView application, click [Add Connections] the Connect dialog displays. Select FactoryTalk Service under the ‘To Service’ section.
  2. Enter the parameters and click [Test Connection]. If all the details are valid, the “Connection Success” message displays.
    Test Connection
  3. Verify the list of InfluxDB tags available under Factory Talk Service model.
    InfluxDB Tags
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal