Verify OPC UA Tags
- Log in to DataView application, click [Add Connections] the Connect dialog displays. Select ‘FactoryTalk Service’ under the ‘To Service’ section.
- Enter the parameters and click [Test Connection]. If all the details are valid, the “Connection Success” message displays.Test Connection
- The new tags from OPC UA Data provider displays under the FactoryTalk Service model. Select the desired tags to generate Storyboard.OPC UA Tags
Provide Feedback