Certificate
Validation Option
When configuring the
OPC UA provider in the InfoPlatform configuration file (see Enable
the OPC UA connector for more details), User can stipulate certificate
validation options for certified connections being made to the server.
Possible options as shown below. Depending on the option selected,
the certificate will be kept in a permanent store, a rejected store
or accepted temporarily.
Property
Name | Description |
---|---|
Reject | Reject
the certificate. |
AcceptOnce | Accept
the certificate temporarily. |
AcceptAlways | Accept the certificate
always. |
Provide Feedback