Change Service Account
Under some situations, user may need to change the InfoPlatform’s service account from the setting made during the installation.
Perform the following steps:
- Open the Services Applet as an administrator from the Windows Administrative Tools applet.
- Open the properties of theFactoryTalk Analytics InfoPlatform Serviceand select theLog Ontab.
- Select theThis accountradio option and enter the name and password of a user who has sufficient privileges to access the resources being used by the InfoPlatform services. These resources may include, for example, FactoryTalk Directory and/or Historians on remote computers.Change Service Account
Provide Feedback