Filtering

Filtering

The RestAPI includes the following Keys that can be used to filter large namespace collections:
  • filterRules
  • maxCount
The following call shows how the filterRules element can be used to filter large collections. In this example, only tags containing the letters “BA:” will be returned:
{"fqn":"Historians.appserhist" , "propNames": ["fqn", "childCount", "type"] , "filterRules": [{"fqn":"BA:"}] }
In the following example, only tags containing either BA:Conc or BA:Active will be returned:
{"fqn":"Historians.appserhist" , "propNames": ["fqn", "childCount", "type"] , "filterRules": [{"fqn":"BA:Conc"},{"fqn":"BA:Active"}] }
Finally, the following call shows the use of the maxCount key to limit the result to 10 items. The maxCount and filterRules keys can be used in conjunction. When used together, the maxCount filter is applied to the result returned after the filterRules filter has been applied.
{"fqn":"Historians.appserhist" , "propNames": ["fqn", "childCount", "type"] , "maxCount": 10 }
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal