InfoPlatform Service Installation Package
NOTE:
Ensure that the following packages are installed before installing InfoPlatform.
The install file is named with the following format:
- Download the FactoryTalk Analytics InfoPlatform Service.M.m.r.bbbb.msiWhere M.m.r.bbbb is the version number of the service:
- M: major
- m: minor
- r: revision
- bbbb: build number
IMPORTANT:To install FactoryTalk Live Data, install “FactoryTalk Service Platform” as needed.
FactoryTalk Analytics InfoPlatform Service depends on a number of other software products whose installation media are not included with this product. The paragraphs below identify these products and their installation media. Prior to installation, check if they are already present on the target system. Unless otherwise indicated, the following can be found on the installation media for FTHistorian at the locations indicated.
NOTE:
Names and exact locations may differ depending on the version of FTHistorian being used.
NOTE:
If FTServicePlatform is already installed, user must apply the FTSP patch. Refer to KB RAID 1092336:
https://rockwellautomation.custhelp.com/app/answers/detail/a_id/1092336
- FactoryTalk Service Platform, FactoryTalk Directory (Note: FTDirectory may be installed on a separate computer)Redist\6.00.00-FTServices\setup.exe
- OSI PI SDKRedist\PISDK\setup.exe
- OSI AFClientRedist\Enterprise\AFClient_x64.msi
- OSI PI System Management ToolsRedist\PISMTSetup\PISMT3.msi
Provide Feedback