Typical Architecture
The following diagram shows a typical architecture of the FactoryTalk Analytics InfoPlatform Service environment.
Typical Architecture
![](/content/dam/dita/en/factorytalk-analytics-dataview/4-01-00/infoplatform-guide-01/overview/typical-arch.png/_jcr_content/renditions/original)
Role | Description |
---|---|
FTHistori | A computer with the following components installed: Required:
Optional
NOTE:
Alternatively, FactoryTalk Directory may be installed on a separate computer. |
OpcDa | A computer with the following component installed:
|
FTClients | A computer with the following components installed:
|
FTA InfoPlatform Service | A computer with the following components installed:
|
Provide Feedback