Install FTServicePlatform
NOTE:
If FTServicePlatform is already installed, user must apply the FTSP patch. Refer to KB RAID 1092336:
https://rockwellautomation.custhelp.com/app/answers/detail/a_id/1092336
To connect InfoPlatform with Factory Talk Live Data or Historian install the following:
- Before installing, check if FactoryTalk Service Platform is already installed on the computer.
- To install the service platform, run the setup from the media as specified in the section.
- To confirm installation, launch Windows Control Panel and select the Programs applet.Verify Installation
Provide Feedback