Troubleshooting FactoryTalk InfoPlatform Service
The following sections describe troubleshooting methods for FactoryTalk InfoPlatform Service issues that may occur during installation and configuration.
Scenario 1: FactoryTalk Analytics InfoPlatform Service fails to start:
There are several reasons this may happen. Here are some things to focus on first:
- Is the service account valid?
- Has the service account been given “Logon as a service” right?
- Does the service account have access rights to the FTDirectory?
To provide the service account “Logon as a service” rights, perform the following steps:
- Navigate to Group Policy Object Editor > Local Computer Policy.
- In the console tree, navigate to Computer Configuration > Windows Settings > Security Settings > Local Policies >User Rights Assignment.
- In the details pane, double-click Log on as a service.
- Click Add User or Group, and then add the appropriate account to the list of accounts that possess the Log on as a service right.
Scenario 2: Web Browser fails to connect to
http://<machinename>:<port number>
- Is InfoPlatform using HTTPS?
- Is the port number correct?
- Is FTSecurity enabled?If FTSecurity has been enabled (which it is by the default installation), user will not be able to access the web services using a browser.To disable FactoryTalk Security, comment out the following element in the infoPlatform section of theRA.InfoPlatform.WindowsService.exe.configfile:<!--SecurityProvider assembly="RA.InfoPlatform.ClaimsProvider.FactoryTalk" type="RA.InfoPlatform.ClaimsProvider.FactoryTalk.ClaimsProvider"><Parameters><add name="SecretKey" value="GQDstcKsx0NHjPOuXOYg5MbeJ1XT0uFiwDVvVBrk" /><add name="OperatorsGroupName" value="FTAnalyticsInfoPlatformOperators" /></Parameters></SecurityProvider-->(OR) Use a tool such as Postman to make web service calls that include headers. All Web Service calls will need to include header fields containing a user name and password associated with a user permitted to access the web service. This user will need to belong the FTAnalyticsInfoPlatformOperators Group.
Scenario 3: User cannot connect to InfoPlatform in DataView application
- Is InfoPlatform using HTTPS?
- Is the port number correct?
- Is FTSecurity enabled?To enable FactoryTalk Security, add (or uncomment) the following element in the infoPlatform section of the RA.InfoPlatform.WindowsService.exe.config file:<SecurityProvider assembly="RA.InfoPlatform.ClaimsProvider.FactoryTalk" type="RA.InfoPlatform.ClaimsProvider.FactoryTalk.ClaimsProvider"> <Parameters> <add name="SecretKey" value="GQDstcKsx0NHjPOuXOYg5MbeJ1XT0uFiwDVvVBrk" /> <add name="OperatorsGroupName" value="FTAnalyticsInfoPlatformOperators" /> </Parameters> </SecurityProvider>If FactoryTalk Security is enabled, ensure to provide a user name and password associated with a user permitted to access the web service when creating the connection in DataView. The user will need to belong the FTAnalyticsInfoPlatformOperators Group.
Provide Feedback