Attributes Tab

Attributes Tab

You can create other Attributes for the selected User by clicking the Attributes tab. For example, a phone number or address associated with the User.
  1. Enter the Name of the Attribute in the Key field and the Value of the Attribute in the Value field.
  2. Click [Add] in the far right column to add a new Attribute.
  3. Click [Delete] in the far right column to delete an Attribute.
  4. Click [Save] once you are finished configuring the Attributes for this User. The saved Attribute will display in the list.
    NOTE:
    Any edits made on this page will not be stored until you click [Save].
    Attributes Tab
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.