Create Users

Create Users

To create a User, follow these steps:
  1. Click Users in the left hand panel.
  2. The User Menu displays. Click [Add User] on the right side of the empty User list.
  3. Enter the username of the User you want to create. The username and email are required fields. Fill out the other fields as desired.
    IMPORTANT:
    If the [User Enabled] field is not set to ON, the User will not be able to access the application.
    Add User
  4. Click [Save] to create the User. You will then be directed to the User Management page for the User you have created.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal