Group
Membership
This section will
list all the Groups that the User is a member of. If you would like
to leave a specific Group, follow these steps:
- Select the Group you would like to leave from the list in the Group Membership so that it is highlighted.
- Click [Leave] in the upper right corner of the box.
- The Group will then disappear from the list.
Provide Feedback