Sessions Tab

Sessions Tab

When a User is selected, there is a Sessions tab that will allow you to view the Sessions that the User is currently logged into. The Sessions list will display the following information about each logged into Session and Last Access:
  • From IP
  • Session Start
  • Clients
  • Actions
  • Last Access
Click [Logout all sessions] to log the User out of all the Sessions that are currently logged into.
Sessions
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.