Authenticator

Authenticator

The Authenticator menu item allows the user to set up OTP if they desire. This will only show up if OTP is a valid authentication mechanism for your realm. Users are given directions to install FreeOTP or Google Authenticator on their mobile device to be their OTP generator. The QR code the user see in the screenshot can be scanned into the FreeOTP or Google Authenticator mobile application for nice and easy setup.
Authenticator
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.