Log
The Log menu of the User profiles is only accessible if the Admin has turned on event logging using the Manage > Events > Configure in the Analytics Security Admin Console.
To access the Account Log, click Log in the left hand panel. A table will appear displaying all the transactions related to the User. The most recent transactions appear at the top of the table. This information is useful when auditing or troubleshooting. The information that is available includes:
- Date
- Event
- IP address
- Client
- Details of the transaction
Log

Provide Feedback