Assumptions

This guide does not cover the installation of the other FactoryTalk Analytics application.
For Windows installations the scripts will need to manage the Windows service for Security Provider and must run from CMD.EXE session with either admin or elevated privileges.
IMPORTANT:
If the PostgreSQL database is already created in postgres machine then skip this step.
The PostgreSQL database is required for Security Provider. If the database server is running on a different host machine than Security Provider, the PostgreSQL Command Line Tools must be installed on the same machine as the Security Provider. The setup scripts use the PSQL command for some database and server setup.
Additionally for new installations the guide assumes that PostgreSQL has been installed and the user has an admin account to create new user and a new database.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.