Single Host/Private Network
When everything is installed in a single host in private network you will only need to have a single certificate generated and signed from a user managed CA. The public key can be shared with users or pushed to users to allow the user’s browsers to trust the FactoryTalk Analytics applications.
Single Host/Private Network
![](/content/dam/dita/en/factorytalk-analytics-security-provider/4-00-00/adv-install-win/introduction/security1.gif/_jcr_content/renditions/original)
Provide Feedback