Prerequisites
- PostgreSQL.
- 7-zip recommended to unzip files. Download and install the 64-bit version of the software from:https://www.7-zip.org.
- SSL certificates.Rockwell Automation recommends using certificates signed by a certificate authority. If none are available at the time of installation, you may create a temporary certificate using OpenSSL.
- OpenSSL - required to create certificates. To generate SSL Key and Certificate, refer to “Pre-Installation Steps” and “Enable SSL for Security Provider” for instructions.
- A recent version (e.g. v1.1.1a) of OpenSSL for Windows is installed on the system. The recommended OpenSSL distribution is the Shining Production OpenSSL-Win64-Light.NOTE:The vcredist_64.exe is a requirement for the 64-bit version of Shining Light Productions version of OpenSSL. The Shining Light Productions OpenSSL is built using Visual Studio 2017. The download can be found with the following URL.https://support.microsoft.com/en-us/help/2977003/the-latest-supported-visual-c-downloads
Provide Feedback