Private Network
When using multiple hosts, it will be necessary to specify the host FQDNs or URLs.
Private Network
![](/content/dam/dita/en/factorytalk-analytics-security-provider/4-00-00/adv-install-win/setup-sec-prov/security7.png/_jcr_content/renditions/original)
The following overrides would be appropriate for this deployment scenario:
fta-setup-env Setting | Override Value |
---|---|
SECURITY_PUBLIC_HOSTNAME | host2.acme-int.com |
DATAVIEW_PUBLIC_HOSTNAME | host2.acme-int.com (for future deployment) |
FLOWML_PUBLIC_HOSTNAME | host2.acme-int.com (for future deployment) |
EDGE_UI_PUBLIC_HOSTNAME | host3.acme-int.com |
EDGE_SERVICES_PUBLIC_HOSTNAME | host3.acme-int.com |
Provide Feedback