Public Network
When using multiple hosts it will be necessary to specify the host FQDNs or URLs. In this case the public and not internal FQDNs need to be used.
Public Network
![](/content/dam/dita/en/factorytalk-analytics-security-provider/4-00-00/adv-install-win/setup-sec-prov/security8.png/_jcr_content/renditions/original)
The following overrides would be appropriate for this deployment scenario:
fta-setup-env Setting | Override Value |
---|---|
SECURITY_PUBLIC_HOSTNAME | security.acme.com |
DATAVIEW_PUBLIC_HOSTNAME | - |
FLOWML_PUBLIC_HOSTNAME | - |
EDGE_UI_PUBLIC_HOSTNAME | edge.acme.com |
EDGE_SERVICES_PUBLIC_HOSTNAME | edge.acme.com |
Provide Feedback