Review
the fta-setup-env Script
The scripts
use a configuration file called fta-setup-env.cmd. This file defines
settings used by the scripts to execute and to configure the Security
Provider. Refer to Table A-1.
NOTE:
Ensure that the psql path
is set in the
fta-setup-env.cmd
file.
Based on the type of installation and the version being installed,
the paths may vary. For example with PostgreSQL 13: set PSQL="C:\Program Files\PostgreSQL\13\bin\psql.exe"
Provide Feedback