Run-fta-setup-vault-store
This step is used to encrypt the keystore passwords. The script will create a vault store for securely storing the keystore and key passwords and will replace plain keystroke and key passwords. The first argument to the script is a password for the vault store.
- Execute the following command to encrypt the keystore and keypassword:fta-setup-vault-store.cmd <vault-store-password> <keystore-password> <key-password> <trust-store-password>
- 1st argument (vault-store-password) in the script is a password for the vault store.Define the password. For example: Passw0rd01
- 2nd argument (keystore-password) is the keystore password.
- 3rd argument (key-password) is the certificate key password.
- 4th argument (trust-store-password) is the truststore password.For example: fta-setup-vault-store.cmd Passw0rd01 Rockwell@1234 Rockwell@1234 Rockwell@1234NOTE:After adding the vault store and encrypting key and keystore password, this script will restart the Security Provider service.
Provide Feedback