Extract the FactoryTalk Analytics Security Package

Extract the FactoryTalk Analytics Security Package

IMPORTANT:
Use 7-Zip file archiving software to extract the Zip files in the following steps.
NOTE:
Depending on how you extract files, the paths may vary. If the files are extracted to a different folder other than the folder shown below, the folder/path instructions may be different for your machine.
  1. Extract the
    FTASecurity-<version>.zip
    file located in the
    C:\<Install_Directory>\FTASecurity
    folder to its current location, if FTASecurity is planned to be installed in the same machine.
NOTE:
If the FTASecurity Provider is already installed, it is recommended to use the existing FTASecurity
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.