openssl.cnf
The openssl.cnf file
contains advanced configuration settings for the OpenSSL command
line tool. In most cases it should not be necessary to make any
changes in this file. Care should be taken with making changes to
this file as the scripts make some assumptions about the default
settings and any changes could break the scripts.
Provide Feedback