Install
OpenSSL
OpenSSL is used to
generate all of the keys used for the CA and for the signed certificates.
User should have a recent version installed. The more recent versions
will have the latest bug and security vulnerability patches. OpenSSL
version 1.1.1 is the Current Stable and Long Term Support (LTS)
version.
For Windows there are a number of distributions
available. The distribution available from Shining Light Productions
is recommended as it tends to be well maintained.
https://slproweb.com/products/Win32OpenSSL.html
Provide Feedback