SSL Settings
The default configuration for the Analytics Security Provider server requires the use of SSL for external connections. If the Analytics Security Provider service or any of the FactoryTalk Analytics applications are used outside the local network, then the servers and the Analytics Security Provider configuration should use HTTPS.
- Login in as security-admin.
- Click the [Login] tab.
- Select [all requests] from the Require SSL drop-down list to enable strict SSL requirement for all requests.SSL Requirement
- Click [Save] to save the changes.
Provide Feedback