Enable Kerberos Authentication in Firefox Browser
Perform the following steps to configure Kerberos in firefox browser:
- Open the browser and enter about:config.
- Click [I accept the risk].Configure
- The URI .mydomain.org must be allowed in the network.negotiate-auth.trusted-uris config option. For example:https://<FQDN-hostname>:<port number>/AnalyticsDataView
- Add the available client URLs (DataView, Edge or DataFlowML URLs) in the config option.
Provide Feedback