Public Network with Reverse Proxy and HTTPS Termination
This scenario is identical to the previous scenario. The difference is that the reverse proxy is doing SSL termination. The Security Provider configuration uses the public URLs, so the Security Provider configuration is the same. The configuration for the reverse proxy will be different.
Public Network - HTTPS Termination
![](/content/dam/dita/en/factorytalk-analytics-security-provider/4-00-00/adv-install-linux-02/images/Security10.gif/_jcr_content/renditions/original)
The following overrides would be appropriate for this deployment scenario:
fta-setup-env Setting | Override Value |
---|---|
SECURITY_PUBLIC_URL | https://analytics.acme.com/security |
DATAVIEW_PUBLIC_URL | - |
FLOWML_PUBLIC_URL | - |
EDGE_UI_PUBLIC_URL | https://analytics.acme.com/edge-ui |
EDGE_SERVICES_PUBLIC_URL | https://analytics.acme.com/edge-services |
Provide Feedback